3/16/2010 2:39 PM | |
Joined: 3/21/2006 Last visit: 10/4/2024 Posts: 10229 Rating: (1181) |
Hello, Can you attach here some sreens with this critical error? Best regards, Hristo Mihalev |
3/16/2010 4:32 PM | |
Posts: 3 Rating: (0) |
My installation is in Italian. This is the screen when I try to uninstall from add/remov application in win XP. |
3/22/2010 9:17 AM | |
Joined: 3/16/2010 Last visit: 4/12/2024 Posts: 9 Rating: (0) |
No news about my problem? |
4/8/2010 9:59 AM | |
Joined: 12/4/2007 Last visit: 1/5/2024 Posts: 26 Rating: (0) |
Hello : What meaning you have in the screen ? Best regards |
4/9/2010 12:17 PM | |
Joined: 3/16/2010 Last visit: 4/12/2024 Posts: 9 Rating: (0) |
There are some uninstall tool? |
4/29/2010 9:02 AM | |
Joined: 8/17/2008 Last visit: 9/19/2024 Posts: 6 Rating: (1) |
Hello, I am meeting the same problem when I want to uninstall older version SCOUT 4.1.2.0. When I start installation of upgrade to SCOUT 4.1.4.1, system recognizes older version but uninstallation crashes with message ERROR Uninstall SIMOTION SCOUT - setup terminated. I have tried to uninstall older version via standard routine Add/Remove programs in Control Panel and also via Setup.msi located in SCOUT DVD /CD2 as you mentioned, both without success. I have used third party program Revo Uninstaller to uninstall older SCOUT Version from my PC, it has uninstalled physically older SCOUT and cleanup all SCOUT inputs in Windows system registry but result is same. When I start new upgrade installation, system recognizes again older version and stops installation. I have also tried to reinstall older SCOUT 4.1.2.0 - with success, but when I want to do upgrade to 4.1.4.1 - installation crashes with the same message. Is there any hint where is problem? Thanks for help. Mike AttachmentScreens.zip (383 Downloads) |
11/1/2012 3:56 PM | |
Joined: 3/2/2007 Last visit: 10/4/2024 Posts: 936 Rating: (5) |
hy sirs, how did you solve this problem? thank you |
... thank you ... |
|
11/5/2012 2:19 PM | |
Joined: 11/15/2006 Last visit: 5/7/2021 Posts: 1319 Rating: (172) |
The second last step is following the FAQ 189025: http://support.automation.siemens.com/WW/view/en/189025 The last one: 'Format C:\' |
Have Fun! |
|
Follow us on