Industry Online Support
Technical Forum
1/28/2014 12:30 PM | |
Joined: 8/19/2013 Last visit: 8/26/2024 Posts: 148 Rating: (11) |
Hello whoright, please have a look to the technical information of the 317 PLC (point CPU-blocks) http://support.automation.siemens.com/WW/view/en/36816526/td The maximum no of blocks in the plc is 2048 - so this is the max. amount Please compare PLC 319 this one is able to handle 4096 blocks ... http://support.automation.siemens.com/WW/view/en/36816536/td Regards |
Follow us on