8/29/2015 6:08 PM | |
Joined: 11/9/2009 Last visit: 2/13/2024 Posts: 1 Rating: (0) |
I also have same problem and there is nothing left to do to solve the problem |
8/30/2015 6:11 PM | |
Posts: 1058 Rating: (93) |
Thanks for sharing. Maybe you should report it to Siemens support, so that they will remove that bug in future versions. regards |
10/21/2015 9:39 PM | |
Posts: 6 Rating: (1) |
I've got the same problem and have raised it with Siemens Tech Support - will advise if I get any joy! |
2/3/2017 7:22 AM | |
Joined: 2/27/2012 Last visit: 5/19/2024 Posts: 29 Rating: (0) |
Hi,I was facing same issue..changing the datetime of the pc solved my issue. Thank you.... |
3/15/2018 9:25 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by Ghazal Ghayem is split to a separate thread with the subject An internal consistency error has occurred. Best regards |
Follow us on