12/24/2023 7:34 AM | |
Joined: 12/18/2014 Last visit: 7/15/2024 Posts: 33348 Rating:
|
Please upload your LSC program as a ZIP file. |
12/24/2023 9:02 AM | |
Joined: 10/7/2021 Last visit: 1/14/2024 Posts: 6 Rating:
|
It is a part of the programm
AttachmentCircuit T5-1 Molen.zip (246 Downloads) |
12/24/2023 2:02 PM | |
Joined: 12/18/2014 Last visit: 7/15/2024 Posts: 33348 Rating:
|
You only uploaded a part of the program and didn't write which counter it was about. So I can only guess what you did wrong. In any case, in this uploaded program you have no connection between the “Start Value” parameter of the B009 counter and the HMI. You also didn't write which HMI it is. If I transfer the "Start Value" parameter of the B009 counter to the VM memory using parameter VM mapping, then load the program into my LOGO! and start the simulation of a Siemens HMI, everything works as desired. See attached video. Which data type did you choose in the HMI? It must be a double word (DWord). AttachmentStart value.zip (222 Downloads) |
12/26/2023 5:51 AM | |
Joined: 10/7/2021 Last visit: 1/14/2024 Posts: 6 Rating:
|
Hi, this is indeed part of the program. As mentioned, I cannot figure out how to stop the minutes Thanks in advance for the effort. AttachmentT5-Smeren V2.zip (262 Downloads) |
Last edited by: Abel64 at: 12/26/2023 05:52:30Last edited by: Jen_Moderator at: 12/27/2023 07:25:47Text formatting optimized. |
|
12/26/2023 6:14 AM | |
Joined: 12/18/2014 Last visit: 7/15/2024 Posts: 33348 Rating:
|
The next problem. You upload only a part of the LOGO! program. But there is no Parameter VM Mapping. And you have problems with overlapping in the VM memory. You use VD0 and also V-Bits of the VB0 (V0.0 - V0.7). But this bits are a part of the VD0. VD0 = VW0+VW2 = VB0+VB1+VB2+VB3 = V0.0 - V3.7. AttachmentLOGO! Bit, Byte, Word and DWord.pdf (280 Downloads) |
Follow us on