10/23/2016 9:18 PM | |
Joined: 2/6/2015 Last visit: 5/31/2024 Posts: 58 Rating: (19) |
I myself tested it with available resources. |
Kaushal Kumar Joshi |
|
10/24/2016 7:34 PM | |
Joined: 10/25/2007 Last visit: 2/28/2023 Posts: 25 Rating: (3) |
Thank You all for advices. I will be next week again on the machine, and i will do same more tests. We compile/master reset/download with Update 8 and Update 9, and it act same. No difference. We tried with another two PG with Update 8 and Update 9 and the results are same. @KaushalKumarJoshi on which network are you connected? Profibus or Profinet? Are you going with command Online or Extender Online? We have S7-400 (with sys diagnose FB), 10 ET200, 10 Scalans switchs, 6 Panels with sys diagnose, safety S7-300 and safety encoder on same Profinet network. We connect on Profinet. Communication is fine, but can not go online or online&diagnose command with nodes after IE/PB link. From sys diagnose on Panel we can see nodes after IE/PB link, but not from TIA portal. |
This contribution was helpful to1 thankful Users |
Follow us on