10/19/2018 8:35 PM | |
Joined: 10/6/2018 Last visit: 3/17/2022 Posts: 16 Rating: (1) |
Hi, I would to know if it is possible to update firmware of a CPU 314C 2DP, exactly a 6ES7314-6CF00-0AB0, to be supported in TIA. I think is v1.0 originally. https://support.industry.siemens.com/cs/ww/en/view/12019198 Is it possible to update or it is too old to update? I have read that sometimes a CPU is upgradeable but it doesn't work well at all. And other question. I downloaded the excel with S300 CPU's supported by TIA, and there are only 2 314C 2DP. 6CG03 and 6CH04. Only v2.6 and v3.3 are supported in TIA? Here: https://support.industry.siemens.com/kompatool/pages/main/index.jsf?sitc=wwdfi10002 These are the only CPU's that are supported in TIA? Or is it possible to update other versions? Thank you so much a regards |
Last edited by: MiguelGT at: 10/19/2018 8:42:53 PMLast edited by: MiguelGT at: 10/19/2018 8:43:15 PMLast edited by: MiguelGT at: 10/19/2018 8:43:45 PMLast edited by: MiguelGT at: 10/19/2018 8:46:33 PMLast edited by: Jen_Moderator at: 10/22/2018 9:43:32 AMOptimized link. |
|
10/21/2018 9:10 AM | |
Joined: 10/6/2018 Last visit: 3/17/2022 Posts: 16 Rating: (1) |
Thanks. But is it possible to update from v1.0 to v2.6 or v3.3? In order to be supported in TIA. Regards |
10/21/2018 9:36 AM | |
Joined: 9/21/2012 Last visit: 7/16/2024 Posts: 4016 Rating: (453) |
This would of been quick and easy search in SIOS using the MLFB number you provided in the first post. From this link, you can see what is the newest possible firmware for your PLC. |
Last edited by: Jen_Moderator at: 10/22/2018 9:44:25 AMOptimized link. |
|
Follow us on