2/26/2015 9:17 AM | |
Posts: 3 Rating: (0) |
Hi All friends! i was trying to update an OS for ktp400 mono HMI. During this process there was a power outrage and hence the update to OS failed. Post this, i could see a simple blue screen on HMI. and it reads " This device contains free software. see OP properties in the control panel for details " on first 3 lines and at bottom " KTP400 Basic Mono PN , boot loader version V1.38 ( 2012-03-27 ) Please help to overcome this problem, Millions of thanks in advance! --------------
Split from Prosave software. |
Last edited by: Min_Moderator at: 2/26/2015 11:41:18 AMNew subject after splitting |
|
2/26/2015 11:54 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (714) |
Hello, try: Read SIMATIC HMI HMI devices Basic Panels When asked boot the panel. Regards, Marcjan |
Problem solved? |
|
8/30/2016 9:56 AM | |
Posts: 1 Rating: (1) |
Hi Markus, I have the same problem. Have you find a solution ? Koen |
1/3/2017 10:19 AM | |
Posts: 1 Rating: (0) |
giúp tôi? |
1/25/2022 11:24 AM | |
Joined: 6/16/2015 Last visit: 4/26/2024 Posts: 29 Rating: (0) |
Hello! Try this instruction 19701610_prosave_1_2_e.pdf https://support.industry.siemens.com/cs/ww/en/view/19701610 chapter 1.3 Resetting the Operating System to the Factory Settings via Ethernet Connection. With best regards. |
Last edited by: Jen_Moderator at: 01/26/2022 08:11:27Optimized link. the collective mind will prevail over common sense |
|
Follow us on