Industry Online Support
Technical Forum
8/17/2012 10:26 AM | |
Joined: 6/5/2009 Last visit: 12/16/2024 Posts: 153 Rating: (0) |
hi dmertens, We're yet to receive update 1 of PCS7 v8.0, but from what I've done I can say that I've used the library filess of PCS7 v8.0 for the traditional channel driver blocks. In APL the PCS7AnIn etc are used but in the traditional library CH_AI etc are used. So I included PCS 7 V7.1 library that I received in the installation DVD of PCS7 v8.0. but it looks like that the problem is'nt getting resolved. is there anything furthur that needs to be done. If possible I'll try it again and let you know. Regards, Grim Reaper. |
Follow us on