3/28/2023 7:57 PM | |
Joined: 3/3/2016 Last visit: 11/6/2024 Posts: 19 Rating: (0) |
Hello together, I am actually working on a similar isue. I d like to upgrade node red because it offers now functionality with the MQTT nodes (dynamic subscription) Now I am not sure from which path I have to start the upgrade, because I think there are two instances of node red on the IOT2050 controller with the example image 1.2.2. One in the root directory and one in the usr directory. I think the second instance will be startet by the systemctl service. Are the customized nodes preserved during the upgrade (node-red-node-intel-gpio-0.0.6-IOT2050)? That nodes are only available in the usr instance. Can the upgrade also be done with the upgrade script for debian os, which is provided by nodered.org? I think that script does an upgrade on nodejs too. https://nodered.org/docs/getting-started/raspberrypi Thanks for your help. Best regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/29/2023 06:31:55New subject after splitting |
|
3/30/2023 11:54 AM | |
Joined: 6/8/2018 Last visit: 11/6/2024 Posts: 110 Rating: (5) |
Hi, Show : https://support.industry.siemens.com/forum/fr/fr/posts/node-engine-update/297008/?page=0&pageSize=10 |
Follow us on