12/13/2012 1:51 PM | |
Posts: 3037 Rating: (192)
|
Hello, I found nothing in the following manual if you can transfer the project from OP15 to PG. Operator Panel OP5, OP15 You must know which program is this project of OP15developed? ProTool or Comtext? OP177B is a Windows-based panel. How is the connection between a Windows-based panel and a SIMATIC S5 set up? http://support.automation.siemens.com/WW/view/en/22585625 Tweety |
12/15/2012 10:10 PM | |
Posts: 4 Rating: (1) |
Hi Tweety, Unfortunately i haven't the backup copy of OP 15 project on the PG. So,how can i download the project from OP to the PG |
1/24/2017 4:53 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
New question published by vipz is split to a separate thread with the subject Software for migration of OP15. Best regards |
Follow us on