1/7/2016 7:10 AM | |
Joined: 5/12/2006 Last visit: 6/5/2024 Posts: 22254 Rating: (2986) |
Hello, the latest FW you find here: https://support.industry.siemens.com/cs/ww/en/view/44442927 You can show if any change in the FW solves you problem. The Password protection is from the project, so if you haven't the password from the project you can't update the PLC with project. Try to update the PLC without project, remove the MMC with the project and insert a empty MMC and update the PLC. Regards Christoph |
Follow us on