10/25/2021 7:03 AM | |
Joined: 9/11/2014 Last visit: 10/31/2024 Posts: 775 Rating: (33) |
Hi, check if you can ping the LOGO!'s on your PC and check the interface LOGO Soft is using. Hope this helps |
11/2/2021 2:11 PM | |
Joined: 8/2/2018 Last visit: 12/16/2023 Posts: 302 Rating: (5) |
Select hardware type to be matching also. |
11/3/2021 3:16 PM | |
Joined: 12/18/2014 Last visit: 11/7/2024 Posts: 34159 Rating: (4255)
|
Sorry, but what has the USB-Port to do with communicating with LOGO! 8.3? |
11/3/2021 3:19 PM | |
Posts: 3 Rating: (0) |
My mistake - it was the ethernet port. |
Follow us on