1/29/2016 5:39 AM | |
Joined: 8/4/2015 Last visit: 5/21/2024 Posts: 8 Rating: (0) |
Hi, I need to upgrade PCS 7 from version 7.0 to version 7.1. I also do some engineering. However, a pop up state that the PO is more than 250 appear when I want to start the runtime (please refer attachment). So, what kind of licence that I need to upgrade the WinCC RC PO to be greater than 250? Currently, I have licence WinCC RC PO (250) Version 7.0. I already bought licence SIMATIC PCS7 V7.1, OS Software Single Station PowerPack (PO 250->Po1.000), but still this licence does not match to upgrade WinCC RC PO 250. Thanks and Regards, Amy AttachmentPO 250 error message.zip (57 Downloads) |
1/29/2016 7:38 AM | |
Joined: 6/14/2006 Last visit: 4/29/2024 Posts: 301 Rating: (60) |
Hi, could you please provide a screenshot of Automation License Manager with all licenses? Myst |
Follow us on