2/13/2015 2:27 PM | |
Joined: 4/9/2010 Last visit: 3/22/2024 Posts: 222 Rating: (33) |
After recent upgrade to V13 SP1 the following parameters changed:
As a result, PLC doesn't communicate with HMI and I can't transfer the HMI file to PC with Runtime. As a workaround, I start runtime on my laptop which creates file I can transfer to the PC with Runtime. This works (sort of) but I can't change Softbus back to ETHERNET. For now, I uninstalled SP1 until someone helps me figure out what to do. Any help is greatly appreciated! Thank you. AttachmentTIA_V13_SP1.pdf (109 Downloads) |
2/13/2015 3:36 PM | |
Joined: 5/28/2008 Last visit: 4/22/2024 Posts: 1343 Rating: (141)
|
Have you tried deleting the connection and create new one with same name? |
2/17/2015 1:16 PM | |
Joined: 5/28/2008 Last visit: 4/22/2024 Posts: 1343 Rating: (141)
|
Are you able to make some screenshots of HW-Config (network view and detail view) |
2/18/2015 9:52 AM | |
Posts: 8946 Rating: (999) |
You may try to install Update 1 for SP1 that was released today. |
Last edited by: IBN-Service at: 2/18/2015 9:53:09 AM |
|
Follow us on