5/25/2014 9:20 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating:
|
Hello Lee.best if you can not download or upload tell us the error that appears maybe we can help you
|
5/25/2014 9:41 AM | |
Posts: 784 Rating:
|
Hello, Change PG/PC address or/and baud rate. Best regards...... |
5/25/2014 10:01 AM | |
Joined: 11/21/2007 Last visit: 7/7/2024 Posts: 2325 Rating:
|
Hello Lee.best The S7-200 CPUs with "CN" in their name are meant for the China Market. However SInce these are less expensive than the So Called S7-200 Classic, these are also available in many Asian Markets. I understand that the major difference between S7-200 "Classic" and S7-200-CN is that "S7-200 CN" does not carry the CE Mark. Since these were specifically for the Chinese market, you can only upload / download to these CPUs if you select your Region as CHina and Language in Microwin as Chinese. You can Do the Programming and Go Online otherwise with ENGLISH. Set your Location to China : Start -> Settings -> Control panel ->Regional & language options -> Location -> China If You have received the S7-200 Program in Chinese, You need to install Chinese Languages in WIndows. To Download / Upload you need to follow the following steps : 1) Open the Program in Microwin 2)Select :Tools->Option ->General tab -> Selectlanguage CHINESE. 3) Download the projectto CPU. ( Itwill downloadwithout any error ). 4) Select :Tools->Option ->General tab -> Selectlanguage ENGLISH. 5) Now you can go onlineand Control the CPU. Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to
2 thankful Users |
Follow us on