4/1/2016 9:01 AM | |
Posts: 1 Rating:
|
Hello all, i m trying to upload program from op17 with prosave, but it showes error "could not open the file" can any one help me. thanks ------------------------------------------------------------------------------------------ |
Last edited by: a.saleem at: 4/1/2016 9:11:10 AMLast edited by: Min_Moderator at: 4/1/2016 11:42:30 AMNew subject after splitting |
|
4/24/2016 5:23 AM | |
Posts: 153 Rating:
|
Hi Try change Device to op7 then backup (i see it in one topic) then if you want restore change to op 17 |
Last edited by: KhanhLe at: 4/24/2016 5:26:23 AM |
|
4/24/2016 5:42 AM | |
Joined: 5/28/2008 Last visit: 7/30/2024 Posts: 4514 Rating:
|
Hello KhanhLe, I don't think so. You can't put wrong device type and expect that the backup process will run. You should put device type correctly in backup, restore or during OS update. Dear a.saleem, Are you sure that you are in transfer mode of OP17? But ensure that you enter this mode without erase the memory of OP17. To do so, you have to press ESC + UP during Startup of the OP. Hope this helps. |
Ayman Elotaify |
|
This contribution was helpful to
2 thankful Users |
4/24/2016 6:35 AM | |
Posts: 153 Rating:
|
I see one people do it, and it's wwork. You cant know it's wwork or not if you dont try it's only take some minute (1,2 minute) and dont loose any thing in panel (in backup mode not resstore, os update). |
Last edited by: KhanhLe at: 4/24/2016 6:37:01 AM |
|
Follow us on