8/24/2022 3:27 PM | |
Joined: 3/2/2007 Last visit: 7/15/2024 Posts: 932 Rating:
|
Kindly, how can we upload the parameters on the following Simoreg K drives ? Which software ? Which cables ? 6RA2232-6DV62-0 , Simoreg K Converter With Microprocessor For Four-Quadrant Drives Connection (B6)A(B6)C, 3-Phase, Ac 380v Controllable Field Rectifier D400/130 Mreq-Gdg 6v62 6RA2225-6DV62-0 , Simoreg K Converter With Microprocessor For Four-Quadrant Drives Connection (B6)A(B6)C, 3-Phase, Ac 380v Controllable Field Rectifier D400/60 Mreq-Gdg 6v62 |
... thank you ... |
|
8/25/2022 3:28 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello, You need either Z1011 or Z1210 board to export 6RA22 drive parameters with RS232 cable & PCIN software. Please refer i needed the supplimentry board Parameter manual for communication of 6 RA 22 Drive via RS 232 port post for more details. Hope this helps. |
Follow us on