3/17/2014 1:49 PM | |
Posts: 510 Rating: (117)
|
Putta, 1. You can use TISOFT to upload the software. It is posted in the SIMATIC 505 Forum, just search on it. 2. TISOFT is a DOS program. I have it running in XP SP3. The attached manual has instructions for installation on Windows 95 in Appendix K. You can extend this to XP. 3. Here is a link to the cable pin out: /tf/WW/en/Posts/20320 4. Section 11.5 has instructions for Saving the Controller Memory to Disk Good Luck billwest AttachmentTS505-8101-7.pdf (952 Downloads) |
This contribution was helpful to1 thankful Users |
3/17/2014 2:21 PM | |
Joined: 9/27/2006 Last visit: 7/2/2024 Posts: 12266 Rating: (2674) |
Hello Putta; Have a look here: Manuals for TI505: Programming software for the Simatic (TI) 505 series:
SIMATIC 505 TISOFT2 Release 6.3 Look at chapter 11 for information on Auxiliary functions: - saving PLC memory to disk (AUX 42, 60-67) - reading and writing EPROMs (AUX 84)
FasTrak SoftWorks, Inc.: PLC WorkShop Suite for Siemens It is possible to download a demo version from FastTrak. Manual: SIMATIC 505 SoftShop for Windows Rel. 3.0 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 3/17/2014 2:24 PMLast edited by: dchartier at: 3/17/2014 2:22 PMLooks like Bill is still quicker on the draw!| |
|
This contribution was helpful to1 thankful Users |
3/17/2014 3:33 PM | |
Posts: 510 Rating: (117)
|
The Demo Version from FasTrak, does not communicate with the controller and only displays the first 25 networks of logic. Here is the link to download TISOFT /tf/WW/en/Posts/37531 Enjoy, billwest |
This contribution was helpful to1 thankful Users |
6/1/2014 8:45 PM |
|
Posts: 114 Rating: (12) |
I hope it may help u /tf/WW/en/Posts/37531
|
Follow us on