2/16/2017 11:41 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985) |
Hi, Uploading only possible, if the Transfer of the current project file from the configuration computer to the operating unit must be performed using the Upload option "Enable backtransfer". So if the option was set then yes, if not then no. https://support.industry.siemens.com/cs/ww/en/view/21907703 Regards |
This contribution was helpful to1 thankful Users |
Follow us on