5/26/2016 10:22 PM | |
Posts: 58 Rating: (0) |
Hi Experts I need upload a program that was downloaded with V10.5 . I don't have a original program . I only have a V13 In one topic in this Fórum I Read that program with V10.5 only have Upload with V10.5 , in other topic I read that V10.5 it can't upload REference: To upload Step 7 TIA V10.5 Program via Step 7 TIA V13 :- open project V10.5 in V13,, is it possible? my questions are the next: 1.- Where I can download a software Tiaportal V10.5? 2.- If I have a Lincese V13 can to work with V10.5 or i need to buy a new lincense? 3.- If I have a V10.5 installed with lincese I can Upload the program? 4.- IF i have a V10.5 installed i can to see a Block OnLine? 5.- If I have a V10.5 installed I can to work with a Watch Table? 6.- If i don't have a original program what i can do to modificate a program V10.5? |
6/2/2016 4:47 PM | |
Joined: 7/7/2010 Last visit: 9/27/2024 Posts: 15239 Rating: (2420)
|
Contact your local Siemens distributor / applications engineer and get a copy of V10.5 SP2. Create a virtual machine and install it there in WinXP (it will not run on Win7-64). XP Mode works as does virtual PC and VMware. In V10.5, you can use the ONLINE ACCESS to see the blocks on the PLC. From there, you can drag them into a PLC you add to a project. Once you have all the blocks, get the tags, watch table, and anything else you can grab via drag and drop. Now look inside the tag table for clues about the hardware configuration. Is there a hardware interrupt OB? If not, you do not have to worry about hardware leading/trailing edge detection. Is there PTO/PWM/HSC configured and used? If so, can you guess how it is configured, maybe using an O-Scope to look at the signal, and compare how it is counting, or creating pulses. Now you are about as ready as you can be to configure your PLC in the project. Use the same PLC name, ip address, subnet mask, and such. Save your project!!! Compile / rebuild all. Fix any errors. Save/close. Now you need V11 to open V10.5 and convert it!!!!! If you do not have a memory card, get one so you can update the Firmware to 2.2. Now update your Project PLC to firmware 2.2 using V11 (which you can use because you have the V13 license). Compile, save. Close. Open V13, and open the V11 project. Compile. This next step is the point of no return. Download, start and evaluate performance. Change as needed to return back to service. Make any needed updates to meet your revised needs. Smile.
|
science guy |
|
Follow us on