10/28/2022 10:57 AM | |
Joined: 8/3/2009 Last visit: 7/10/2024 Posts: 13259 Rating:
|
Hello I think the Smart Panels are made for the ASIA marked. SO you will find not much information here. I think they are programmed with WinCC flex 2008 Sp4 ??? (I´m not sure) If yes there is a little chance that someone has used the backtransfer option while loading. But if it was not used the last time it was loaded then you cannot do a full download from the panel. then only a Backup is possible. (LINK) Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on