5/7/2019 2:57 AM | |
Joined: 9/27/2006 Last visit: 9/10/2024 Posts: 12282 Rating:
|
Hola Mario; Los participantes en este foro de Siemens vienen de muchos paîses, donde no todos entienden el español. Para facilitar las discusiones hemos escogido el ingles como idioma de intercambio. Haznos el favor de escribirnos en ingles a tu prôxima visita. Hello Marioñ Members on the Siemens forum come from many countries, and many do not understand Spanish. We have chosen English as an exchange language to facilitate our discussions. Plese do us the favor of writing in English on your next visit. I am afraid that the HMI panel KTP900 that you are using is a Basic Panel, and will accept backup/restore features of the program only with the Prosave tool. The *.psb file produced is compiled and can only be used to restore the program on a HMI panel with the same part number. It cannot be opened or modified in WinCC v1x. You can check this out in the manual for the Basic Panels )second generation: https://support.industry.siemens.com/cs/us/en/view/90114350 Hope this helps, Daniel Chartier Translation from the Spanish text:
|
Last edited by: dchartier at: 05/07/2019 03:07:51 |
|
This contribution was helpful to
2 thankful Users |
Follow us on