9/15/2020 10:21 AM | |
Joined: 4/24/2006 Last visit: 6/28/2024 Posts: 8698 Rating: (1160)
|
Hello, What is the reason to upload from OP73? Best regards, Wizard |
9/24/2020 11:15 AM | |
Joined: 8/3/2009 Last visit: 6/27/2024 Posts: 13163 Rating: (1669)
|
Hello jrdavisim what do you mean with upload (this word leads often to misunderstanding) Do you want to load a project from Engineering PC to the Panel? or Do you want to load the runtime Project out of the Panel to a PC? -> in this case its only possible if you had activated the Backtransfer but the OP73 does not support a Backtransfer (LINK) so you could only do a Backup LINK Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on