11/10/2009 2:39 PM | |
Joined: 3/24/2009 Last visit: 8/7/2023 Posts: 406 Rating: (3) |
Hi, I am trying to upload the program from S7200 plc using microwin software v4.0. But i am not able to upload the program.I successfully communicated with plc. I also attached the screen shot of the problem.Kindly help me out from this issue.The program which was stored in the plc developed by chinese may be it is in a format of chinese.So what i have to do? AttachmentS7200_1.zip (150 Downloads) |
All is well :-) |
|
5/6/2010 7:42 PM | |
Joined: 10/7/2009 Last visit: 8/19/2023 Posts: 266 Rating: (92) |
Hi, Now you can download and upload S7-200 CN using MicroWin SP7. You-win |
2/24/2016 12:54 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by siemensexpert is split to a separate thread with the subject S7-200, can't make uploading to the software stored in the CPU. Best regards |
Follow us on