11/8/2010 2:28 PM | |
Joined: 1/4/2007 Last visit: 5/6/2024 Posts: 1117 Rating: (174)
|
post deleted |
Last edited by: Siwarexi at: 11/8/2010 2:36 PM |
|
11/8/2010 2:35 PM | |
Joined: 1/4/2007 Last visit: 5/6/2024 Posts: 1117 Rating: (174)
|
Hello Scope, |
11/9/2010 10:14 AM | |
Posts: 4 Rating: (0) |
Hello Siwaexi, Thank you for answering me. In the topic https://www.automation.siemens.com/tf/WW/en/Posts/48626#top
I don`t understand what does he mean with " measuring range " ? What will happen if the char. value of the load cell is 2mv/v and i set the char.value of siwatool to 4mv/v ? I red the Quick Quide.I understood some points ,please correct me if i was wrong. I realized that If i make adjustment using calibration weight, then I don't need to use adjustment digit 0 and 1. but, i didn't understand this paragraphs:
How can i choose the resolution in siwatool?
How can I adjust the parameters manually ? |
11/9/2010 12:16 PM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
HI Scope, First You Download this Manual Basic Data Setting, 1. I don`t understand what does he mean with " measuring range " ? What will happen if the char. value of the load cell is 2mv/v and i set the char.value of siwatool to 4mv/v ? A. You have to see the Characteristics of the Load Cell, for the Liner & correct Responce of the Load Cell you have to put the Characteristics as per the Load Cell Name Plate. are you going to used your System over Weight ? then you have to think about the change the Characteristics. 2. I red the Quick Quide.I understood some points ,please correct me if i was wrong. I realized that If i make adjustment using calibration weight, then I don't need to use adjustment digit 0 and 1. but, i didn't understand this paragraphs:
A. This the Resolution of the Weighing as your Load Cell Weight Increase the Resolution is going to Decrease. the same thing is Explain in the Above Exp. 3.How can i choose the resolution in siwatool?
the same thing Is Explain in the Above. Please Follow the Calibration/ Adjustment Procedure As per the Manual Link. if need then used for theoretical adjustment. |
Ammy |
|
Follow us on