8/18/2015 11:18 AM | |
Joined: 11/30/2011 Last visit: 9/1/2023 Posts: 31 Rating:
|
Hello Everyone, I Required CPU414-4H(6ES74144HM140AB0) firmware v4.5.4. i am unable to download this file from https://support.industry.siemens.com/cs/document/109474703/download-operating-system-updates-v45h-cpu412-3h-cpu414-4h-cpu414-4h-pg-cpu417-4h-?dti=0&lc=en-US link. |
8/18/2015 2:09 PM | |
Joined: 5/12/2006 Last visit: 6/29/2024 Posts: 22290 Rating:
|
Hello,
no i don't attach the FW File here ! If you can Download the FW Version 4.5.7 then i think is better you use this version because the V4.5.4 oís only for backup, the 4.5.7 ist the latest and includes all fixes .
Regards Christoph |
8/19/2015 5:09 PM | |
Joined: 1/28/2009 Last visit: 6/26/2024 Posts: 6841 Rating:
|
Dear friends, I have had the same problem while working with Firefox and discussed that with a member of moderating team. There is a workaround for this problem and it helps downloading from mentioned support website.When I tried to download (4123hj14_v454.exe (1.4 MB)) , the browser tried to access the file with the following link: https://cache.industry.siemens.com/dl/files/703/109474703/att_832823/v1/4123hj14_v454.exe and same error as mentioned.I tried again and replace "cache" with support and the file start downloading. https://support.industry.siemens.com/dl/files/703/109474703/att_832823/v1/4123hj14_v454.exe It works for me.The reason came from the fact that "cache" files are temp and they are not valid for a long time. I hope this helps , Hamid Hosseini |
Follow us on