7/16/2008 1:20 PM | |
Joined: 4/24/2006 Last visit: 6/28/2024 Posts: 8698 Rating: (1160) |
Hello Graeme, Here are some answers:
The USB PC-adapter needs 24 volt, via MPI/Profibus port. A CPU provides this 24 volt. But not all Profibus slaves have a Profibus port that provides 24 volt.
Have a look at this thread: /tf/WW/en/Posts/15455 Best regards, Wizard |
This contribution was helpful to1 thankful Users |
7/16/2008 2:13 PM | |
Posts: 5822 Rating: (411)
|
You are right Wizard, besides the CPU you can only use the PG interface on a RS485 Repeater to supply the MPI Adaptor.. as far as I know. Best regards J_Bell |
4/22/2010 2:49 PM | |
Joined: 1/17/2007 Last visit: 6/17/2024 Posts: 69 Rating: (0) |
Or you can buy a cable from Siemens (you can made it yourself) with additional power supply |
8/31/2014 8:02 AM | |
Joined: 9/1/2005 Last visit: 5/14/2024 Posts: 4101 Rating: (194) |
new questions published by Marsusare split to seperate threads with the subject difference between CP5512 and normal MPI cableand cable for connecting both PLC directly and through profibus. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on