2/15/2018 6:30 AM | |
Joined: 10/22/2011 Last visit: 3/12/2025 Posts: 303 Rating:
|
Dear All, I have 6ES7901-3DB30-0AX0 cable. When I plug the cable into USB port, it is shown under Human Interface Devices in Device Manager. The cable is working fine with S7-200 in Microwin when I select USB in local connections. Now I want to use the same cable with OP177B to upload/download. can anyone tell me how can I use it? as it is displayed under Human Interface Devices , but not under the Serial Port. waiting for reply |
2/15/2018 6:37 AM | |
Joined: 9/21/2012 Last visit: 3/14/2025 Posts: 4324 Rating:
|
OP177B doesn't support PPI connection, only MPI/DP or ProfiNET models are available. You need a PC ADAPTER USB A2 to connect to the display. |
2/15/2018 6:45 AM | |
Joined: 10/22/2011 Last visit: 3/12/2025 Posts: 303 Rating:
|
Can I use this USB PPI Multi master cable for other TP or KTP? |
2/15/2018 6:53 AM | |
Joined: 10/22/2011 Last visit: 3/12/2025 Posts: 303 Rating:
|
please see the attachment, here is is written that PC/PPI cable can be use with OP177B also in Transfer settings of OP177B, it is displaying option for RS232/PPI . what does it mean? |
Follow us on