Industry Online Support
Technical Forum
8/24/2012 2:45 PM | |
Posts: 378 Rating:
|
Hello MvdW, I couldnt understand your question well from the picture please attach your logo program here ( you should make it .ZIP file in order to post here). Regards, |
8/24/2012 3:13 PM | |
Posts: 4 Rating:
|
Hello, Here the is the program where a talking about AttachmentIntratuin Weert 01-08-2012.zip (326 Downloads) |
8/25/2012 6:17 PM | |
Posts: 378 Rating:
|
Hello MvdW , You can not directly acess the analog value via network. You need to make variable mapping for each analog adress. 1. Set different IP adress for Server and Client. 2. Right click Ethernete connection and click Add Connection. 3. Select Connection type (Server or Client) 4.Under data transefer, on ID column select Read if you gonna to read analog output from other device, On Data Length column set 2 for word, On Adress column (on local and remote) type the adress e.g. VB2. 5.Go tools>>VM mapping and select the block and type the adress similar to the adress of Data Transfer (as in step 4.) I have attached a simple program for your referance. Regards, AttachmentMasterSlave.zip (314 Downloads) |
8/29/2012 1:42 PM | |
Posts: 4 Rating:
|
Hello, I does't undertand the way i have to program this. can someone try to explain this to me. grtz from the Netherlands. Manfred vd Waarsenburg |
Follow us on