5/10/2008 2:27 AM | |
Joined: 12/4/2007 Last visit: 5/10/2024 Posts: 7 Rating:
|
My machine tool's control system is 802Dsl V1.4 Sp1 Pro, and drive system is Sinamics S120, I need use absolute linear scale (LC183 Heidenhain with increment signal) for the measuring system. I have seen in NC61, that sinamics s120 support direct linear absolute encoder Endat LC183. But after I use starter to configure the drive, the SMC20's LED turning red, there are four linear scales here, the phenomenons are the same. The attatch is the starter file, Servo 5 and Servo 6 use the absolute linear scale, pls help me see, what's wrong for it? Thank you! For the web can't upload the .rar file, so I change the extend name for .rar to .zip. when open the file, pls first change the extend name from .zip to .rar. AttachmentNewlife.zip (436 Downloads) |
5/12/2008 10:42 AM | |
Joined: 4/18/2006 Last visit: 3/21/2025 Posts: 17 Rating:
|
Did you try to configure the direct system meas from HMI? Without use the Starter? |
Follow us on