6/24/2024 9:34 AM | |
Joined: 5/29/2024 Last visit: 7/4/2024 Posts: 21 Rating: (2) |
Hi jthyge1! Text lists in faceplates can only be used within the scope of the faceplate. You cannot use "global" text lists in a faceplate. This is indicated in the manual: https://support.industry.siemens.com/cs/ww/en/view/109760739/113491708683 You create the faceplate lists in the Graphics Designer. Lists that are created in the "Text and graphics lists" editor are not available in faceplates. Faceplate text lists and faceplate graphics lists are only available for the faceplate in which they were created. They are not displayed in the "Text and graphics lists" editor. |
Last edited by: The Helping Hand at: 06/24/2024 13:48:27Link optimized If this Information really helps, you could use the Rate function |
|
This contribution was helpful to2 thankful Users |
Follow us on