Industry Online Support
Technical Forum
10/30/2018 5:38 PM | |
Joined: 12/13/2013 Last visit: 8/30/2024 Posts: 36 Rating: (0) |
Hi, I am commissioning 840D SL, in which i have a 2 channel configuration. I want to do feed disable and nc start disable for both channel sequentially. For this i am using DB21.DBX6.0 and DB22.DBX6.0 for feed disable and DB21.DBX7.0 and DB22.DBX7.0 for NC Start Disable. after enabling these bits i am not finding any effect on the system. All axis are moving and cycle is also getting started. for checking i have forcefully enabled it in OB1 network 7. After checking the status in VAT, these bits are show in off conditions. in cross reference also it show its use at one network only. for your reference i have attached the PLC backup. kindly support. thanks rohit jage unicorn controls AttachmentTool_gri.zip (57 Downloads) |
Follow us on