6/28/2013 1:20 PM | |
Joined: 2/1/2011 Last visit: 9/13/2023 Posts: 186 Rating:
|
Dear viralpatel, For the first time will be using absolute encoder so let me know that encoder on profibus or through card will provide direct angle or pulse count and than we have to process it as angle. secondly please elaborate little that why cant we used the process defined by me. we can do the calculation as told above. Dear manmeet As you said that card will retain the value which means the actual position is retain by me in PLC so after power off and maintenace I still have the value with me so there will not be requirement of home until and unless they rotate encoder in off. I think so same will happen with absolute encoder also(If rotate in power off) |
6/28/2013 1:48 PM | |
Joined: 1/3/2006 Last visit: 10/16/2023 Posts: 726 Rating:
|
No same thing does not happens with absolute encoder. Even if after you power off PLC / encoder it always gives you reading. Every angle will generate certain set of digital inputs and you just cant loose values. Mechanical guys needs to set absolute encoder properly. Say if machine is tilted at zero degrees then absolute encoder shall give you zero degress only and not some other values. This can be done by resetting the ecoder at zero degrees.Once its set properly you are on your way to operate machine properly. Edit: Once set properly, if you take machine into maintenance and during mainteance (Control panel OFF) machine is moved by 30 degrees and then say control panel is swiched ON, you will get value of 30 degrees in PLC. More about absolute encoder overhere. |
Last edited by: manmeet at: 6/28/2013 1:55 PM |
|
6/28/2013 1:57 PM | |
Joined: 11/18/2010 Last visit: 8/5/2022 Posts: 523 Rating:
|
Hi , absolute encoder has more then 10 terminal which you have to connect with DI of PLC and it has fix encoded position set means on 0 to 360 degree it will give binary pulse out to that terminal it give position value so at any position at will give specific fixo/p incaseof encremental encoder it will give pulse as shaft rotating so it will be PLC responsibility to measure it it has nor mally 8 terminal like A/-A,B/-B,Z/-Z and supply wire regards,, viral |
Follow us on