5/21/2017 1:54 AM | |
Posts: 9 Rating:
|
can i use siwarex wp231 directly connected to s7-1215c without siwatool? im still new at this and i cant seem to be able to connect siwares wp231 to my plc. diag light is always red also it keeps telling me when i try to load my program that oline v4.1 and offline v4.0 what should i do? ------------------------------------------------------------------------------------------ |
Last edited by: chie19 at: 5/21/2017 2:24:32 AMLast edited by: chie19 at: 5/21/2017 4:06:46 AMLast edited by: Min_Moderator at: 5/22/2017 1:53:14 PMNew subject after splitting |
|
5/24/2017 11:03 AM | |
Joined: 1/4/2007 Last visit: 7/11/2024 Posts: 1134 Rating:
|
Hello chie19, Yes, you can connect the Siwarex WP231 directly beside the S7-1215C PLC without Siwatool. You can find some Step7 example programs on the internet: https://support.industry.siemens.com/cs/ww/en/view/66825585 “diag light is always red” => What’s about the LC LED? Is this LED also red? If so, the load cell is not connected correctly to the WP231 module and the red DIAG LED goes also on. “it keeps telling me when i try to load my program that oline v4.1 and offline v4.0 what should i do?” I guess the firmware of the PLC has online V4.1, but you selected a PLC with the firmware V4.0 in your TIA Portal project. Best regards Siwarexi |
4/17/2018 12:23 PM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating:
|
New question published by ingenia_clm is split to a separate thread with the subject Connect wp231 module with the plc 1214: It shows protection personal error. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on