1/28/2013 3:15 PM | |
Joined: 5/18/2006 Last visit: 10/21/2020 Posts: 170 Rating: (64) |
Depends on what version of PCS 7 you are using (APL verses Standard Blocks/Faceplates). |
This contribution was helpful to1 thankful Users |
1/29/2013 10:34 AM | |
Joined: 3/14/2008 Last visit: 12/31/2024 Posts: 2156 Rating: (968) |
The difference is that the first one has authorization for "standard library blocks", and the second one isauthorization of apl library blocks". For example...you have twoPID blocks, one from standard library, other from apl. You wantto change a parameter which needs authorization. ForPID in normal library assignnumber 5,to change a parameter of the apl pid , you use number 6. |
If I could help you, you can use the RATE button. Thank you. |
|
1/29/2013 11:47 AM | |
Posts: 4 Rating: (0) |
Thank you for your help cabreytj. |
9/16/2020 7:35 AM | |
Joined: 7/2/2018 Last visit: 12/19/2024 Posts: 16 Rating: (1) |
|
Follow us on