8/15/2016 12:10 PM | |
Posts: 62 Rating: (0) |
I program in PCS7 v8.0,do you have any example about configuring Alarm_8p in CFC? |
Last edited by: nasibe at: 8/15/2016 12:11:51 PM |
|
8/26/2016 10:25 AM | |
Posts: 111 Rating: (15) |
Hello nasibe, I don't know if I understand you correctly, but I try to help. 1. you can define the text via the settings of the EVENT-block (right-mouse menu =>messages) 2. the AV input is for additional information, if you want to use e.g. the analog values as a part of the message, useable as formatted string e.g. @1%4,2f@ ==> the number 1 is the AV1 input, the string formats the value to string in the message. So there can be a using/influence to the message by the AV input. If the DB struct has the correct syntax, you can directly use the DB struct as AV input. 3. If the struct isn't useable as input, there is a need to split the struct and convert the struct-elements. Or you can create/use an new struct in the DB which directly is useable. Further information: SIMATIC Process Control System PCS 7 Advanced Process Library (V8.2 SP1) |
Last edited by: nussbaum at: 8/26/2016 10:31:34 AMLast edited by: nussbaum at: 8/26/2016 10:32:14 AM |
|
8/26/2016 10:54 AM | |
Joined: 10/26/2011 Last visit: 5/3/2024 Posts: 761 Rating: (190)
|
How Mark1707 has described, use the block "event". It is described in the Advanced Porcess Library (APL) manual, chapter 8. Direct to the chapter 8: Link to the APL manual: The block "event" is easy to use and it is developed exactly for that, what you want. |
Last edited by: Thunderstorm at: 8/26/2016 10:55:26 AMSIMATIC PCS 7 - Overview |
|
8/27/2016 7:08 AM | |
Posts: 62 Rating: (0) |
Thanks for your help,I was looking for message properties and I did not know it is so easy to find , thanks again. |
Follow us on