3/2/2012 1:36 PM | |
Posts: 4 Rating: (1) |
Ivo, you should use AJAX. First of all, create XML file with all needed params, then get data from it and use it as you with. Simple example is attached. Regards, Gintaras AttachmentDB.zip (1421 Downloads) |
This contribution was helpful to1 thankful Users |
3/7/2012 7:50 AM | |
Posts: 20 Rating: (1) |
Go to the configuration of the PLC in TIA, and open the 'Web sever' part. The block below the block generator you can define wich files have dynamic content. |
3/7/2012 8:59 PM | |
Posts: 20 Rating: (1) |
Can You attach any example working simple project with AWP commands in javascript? |
Follow us on