Industry Online Support
Technical Forum
5/12/2011 8:49 AM | |
Posts: 2661 Rating: (279)
|
You have to create an Excel based OPC client. See the following FAQ: How do you create an OPC client with Microsoft Excel? Regards |
5/24/2011 6:55 AM | |
Posts: 212 Rating: (12) |
hi, Writing from MS Excel to WinCC Runtime can happen via OPCDA. follow attached link, which provides the application tool using excel for performing writing application. http://support.automation.siemens.com/WW/view/en/44444703 |
This contribution was helpful to1 thankful Users |
Follow us on