6/17/2021 5:35 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, I have added a flow in the attachment of how I successfully managed to subscribe to a changing boolean with 2Hz. The solution is very similar to what you mentioned. The interval value within the Client Node stands for requestedPublishingInterval but sadly it is not being used internally, so you indeed have to pass this value through the Input of the client node as in my example: On the PLC side I would actually set the minimum publishing interval lower than 2Hz, or you might have trouble collecting all changes. Afterwards you should receive a debug message every 500ms: Hope this helps! Attachmentflows (8).txt (916 Downloads) |
Follow us on