8/31/2017 7:27 PM | |
Posts: 2 Rating:
|
Hi All, Problem 1 Using TIA 13 SP1 we are trying to configure a Simocode ProV connected to a 1200CPU. When adding it onto the Profinet network in TIA, the software insists that the Simocode has an input card - which it does not have. It is not possible to delete the self-configured input card. We ended up configuring the Simocode with the Simocode ES software directly without the input card problem. From TIA, we then uploaded from the Simocode but in TIA, it still adds the input card onto the Simocode. Is there a way to get around this? The PLC indicates a device error when connected to the Simocode. Problem 2 [snip] ... Thanks for any help Mike ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 9/1/2017 12:57:29 PMNew subject after splitting Last edited by: CS Moderator at: 9/11/2017 12:19:15 AMsecond question split to a seperate thread |
|
9/11/2017 12:14 AM | |
Joined: 9/1/2005 Last visit: 7/9/2024 Posts: 4101 Rating:
|
Second question published by MikeRave is split to a separate thread with the subject Simocode ProV connected to a 1200CPU - fail to write to the Simocode's cyclic receive bits. Best regards |
My Forum is the place to personalize your profile, |
|
9/26/2017 10:06 AM | |
Joined: 5/17/2010 Last visit: 5/22/2024 Posts: 226 Rating:
|
Hi, I would recommend to get in contact with Siemens Support on this very Special behavior. => email to technical-assistance@siemens.com |
------------------------------------------------------------------------------------------------ |
|
10/16/2017 1:14 PM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating:
|
New question published by Branimir is split to a separate thread with the subject Simocode pro v MR - Problems with hardware configuration. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on