10/19/2016 9:20 AM | |
Joined: 3/2/2007 Last visit: 3/24/2023 Posts: 827 Rating:
|
can we use a sinamics s120 motor module with a cu320 control unit to run an normal asynchronous motor in v/f mode? without any speed feedback from the motor? will we have any errors or alarms? 6SL3120-2TE13-0AA4, SINAMICS S120 DOUBLE MOTOR MODULE INPUT: DC 600V OUTPUT: 3AC 400V, 3A/3A FRAME SIZE: BOOKSIZE INTERNAL AIR COOLING OPTIMIZED PULSE SAMPLE AND SUPPORT OF THE EXTENDED SAFETY INTEGRATED FUNCTIONS INCL. DRIVE-CLIQ CABLE 6SL3040-1MA00-0AA0, SINAMICS CONTROL UNIT CU320-2 DP WITH PROFIBUS INTERFACE WITHOUT COMPACT FLASH CARD 6SL3054-0EH01-1BA0, SINAMICS S120 COMPACTFLASH CARD WITH FIRMWARE OPTION PERFORMANCE-EXTENSION INCLUDING CERTIFICATE OF LICENCE V4.7 1LA7106-4AA11 |
... thank you ... |
|
Follow us on