12/12/2014 1:55 PM | |
Posts: 3 Rating: (0) |
Hello Jerome, there is an application example how to control V20 drives with a S7-1200 PLC via MODBUS RTU. Use the link http://support.automation.siemens.com/WW/view/en/63696870 Regards JuSaKri |
This contribution was helpful to1 thankful Users |
4/14/2015 9:06 AM | |
Joined: 2/23/2015 Last visit: 10/8/2024 Posts: 15 Rating: (2) |
Hi Jerome, Please be sure that parameters P0700 and P1000 is set to '5' Best Regards, Piotr |
4/29/2018 3:39 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by Comtable_1411995 is split to a separate thread with the subject Which parameters must set up to control speed of V20 with S7 1200?. Best regards |
This contribution was helpful to1 thankful Users |
Follow us on