10/7/2016 11:13 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (878) |
How V90 is interfaced to S7-1200? Via profinet, MODBUS etc? Please check below FAQ may help you. |
10/7/2016 11:18 AM | |
Joined: 3/12/2015 Last visit: 11/4/2024 Posts: 537 Rating: (15) |
profinet, and the x8 conector i have cabled like this... |
10/7/2016 12:52 PM | |
Joined: 3/12/2015 Last visit: 11/4/2024 Posts: 537 Rating: (15) |
. |
10/7/2016 1:30 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (878) |
Are you sure you have established profinet communication with PLC? How much is the value in p0922 =? Please refer following FAQ for detailed information. Please go thru the Documentation (1,4 MB) file. Speed Control of SINAMICS V90 with SIMATIC S7-1200 via PROFINET |
Follow us on