6/25/2018 3:54 AM | |
Joined: 9/3/2014 Last visit: 3/7/2024 Posts: 79 Rating:
|
Dear Experts, I'm working in automation project, I've bought next parts: -> SIMOTICS S-1FL6 1FL6052-2AF21-0AA1 - 3AC230V - 1.5kW - NN=3000rpm - M0=4.78Nm - ENCODER TTL 2500 incr/rev - IP65 -> SINAMICS V90 6SL3210-5FB11-5UA0 - 3AC200-240V - 11.0A - 1.5kW - IP20 - 95x170x195(WxHxD) I need to do a Speed Control in a machine, I've connected the v90 and the servomotor, I'm programming in V-ASSISTAN, I can move the motor trought the software, But I can't move the motor trought IO terminals block, I can read the voltage in analog input, but I don't know what is the digital input that let me start the motor, I've combined some terminals to start the motor, but anyway has been succsesfully I've attached some pictures about the configuration I've done, I'l be gratefull if you can help me, Thanks a lot, Regards,
Attachmentv90.pdf (87 Downloads) |
Follow us on