10/18/2019 8:45 AM | |
Joined: 5/13/2016 Last visit: 1/15/2022 Posts: 66 Rating: (5) |
Hi, I've tried to make a rough start on the first part of your question. This is far from perfect, but perhaps enough to get you started? In the first part we have 3 inputs for the analog output selection, exact voltage values need to be set. In the 2nd part I've created some switching logic for the BV valve. This probably needs more interlocks and logic, just see this as a start for expansion If this is something you are looking for and you need more help just let us know. AttachmentVacuum Excavation Truck.zip (206 Downloads) |
10/18/2019 10:52 AM | |
Joined: 5/13/2016 Last visit: 1/15/2022 Posts: 66 Rating: (5) |
Hi Morgs, Try the attachment. Again, this is far from finished, all loose pieces of program to get an idea. I now made the BV1 and BV2 to work inverted of each other. Of course it's also possible to have a seperate timer for it. This way however ensures they are never active at the same time. Regards Luna AttachmentVacuum Excavation Truck.zip (215 Downloads) |
Follow us on