7/11/2020 11:09 AM | |
Joined: 4/14/2019 Last visit: 9/11/2024 Posts: 43 Rating: (0) |
In the same way i tried, In my case i have a Mitsubishi HMI & S7_1200 PLC and Trio Motion Controller running on a same network [Named as No 1] Motion Controller Communicating with PLC as Station 2. Now I want To feed some input values to S7_1200 PLC [ Selected as Station 3] in HMI. For that I run my server block, assigned a data block of Array of 10 Words. As per trailing discussion , DB102.DBW 0 = 400001 DB102.DBW 18 = 400010. So As per that i tagged my IO field as [NW ID].[STN NO].[MB ADDRESS] = 1.3.400001. Which Means that if we feed any value , expecting it will reflect in my DB102 under address DB102.DBW0. Which is not happening., why..?? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/13/2020 07:28:26New subject after splitting |
|
7/13/2020 7:29 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (173) |
Closed cause question posted twice. The second thread with the subject Write a Value from Mitsubishi HMI to S7-1200 PLC via Modbus TCP Interface. is published within the conference SIMATIC Modbus/TCP. Best regards,Jen_Moderator |
Follow us on