Industry Online Support
Technical Forum
8/30/2023 6:52 PM | |
Joined: 10/15/2022 Last visit: 7/6/2024 Posts: 66 Rating:
|
Hello again This program stores the value from the analog input in the first memory and after a certain interval shifts it to the second and then the third memory, filling the rows from top to bottom. On the screen you can see the current value and three stored values, the oldest one on the bottom line and the newest one a few lines higher. Values range from 0 to 1000. The idea and technique taken from Temperature shift for 7 days. A softkey block is in use, an interval timer has been added and a warning has been made if the interval time is too short.
AttachmentValues shifting demo.zip (287 Downloads) |
Last edited by: Andrus_Saar at: 08/30/2023 18:55:02 |
|
This contribution was helpful to
1 thankful Users |
Follow us on