8/8/2017 7:06 PM | |
Joined: 3/14/2008 Last visit: 9/5/2024 Posts: 2094 Rating:
|
Hi, yes that is an option. Make sure you delete the PCS7DiIn for the feedback open and set parameter NoFbkOpen to 1 at the valve block. This make sure an error is not generated when the open feedback is expected. You can also inverse the digital input signal at PV_In at a later point (PCS7DiIn) |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
Follow us on