1/19/2021 10:46 PM | |
Posts: 11 Rating: (0) |
Another question: If you wanted to program so the Valve Opened at a specific time, say opened at midnight for a 10 minute duration then closed, is the best way to do this by implementing a weekly timer? In this case you would select the active days and times, so MTWTFSS On1=00:00, Off1=00:10, or I suppose you would have to have the pulse output specify the Off or end of the cycle? Thanks in advance! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/20/2021 09:51:41New subject after splitting |
|
1/20/2021 9:08 PM | |
Posts: 11 Rating: (0) |
Wow, or is this embarrassingly simple?! Or am I missing something? |
1/20/2021 9:10 PM | |
Joined: 12/18/2014 Last visit: 8/22/2024 Posts: 33606 Rating: (4177)
|
Maybe this is what you want ...
AttachmentTime_controlled_valves_0BA8.Standard.zip (343 Downloads) |
This contribution was helpful to1 thankful Users |
1/20/2021 10:59 PM | |
Posts: 11 Rating: (0) |
I think I got it by changing the inputs on B001 with the M8 on 1 and Timer on 2. Seems to work now when the weekly timer comes around. |
Follow us on