4/12/2016 3:34 PM | |
Joined: 11/29/2011 Last visit: 7/17/2024 Posts: 1358 Rating:
|
Hi, That is funny one... The issue caused by a feature in @PCS7TypicalsAPLV8.PDL. Have you tried to use a different variant of ValMot block icons? Maybe try to open the above PDL to identify what variant you need, or create your own block icon based on PCS 7 Programming Instructions for Blocks V7.0 and higher. There is an FAQ about as well: How do you create your own block icons with SIMATIC PCS 7? PS: as I recall this feature come with APL V8, so as I remember the block icons from APL V7 works without this feature. |
Last edited by: MicroMan at: 4/12/2016 3:43:25 PMmark1507 was faster!!! - What you read here, please check with manuals and your requirements. |
|
This contribution was helpful to
2 thankful Users |
4/12/2016 3:44 PM | |
Joined: 3/14/2008 Last visit: 7/25/2024 Posts: 2079 Rating:
|
As I understand, this is basic functionality of the block icons... It will change it's direction when opening or closing. The reason is because the color blind operators can see a valve is changing it's state... If you set block icon numbers 3 or 4 (since v8.x), then you have valves which do not change their direction. |
Last edited by: Oreca at: 4/12/2016 6:41:54 PMAdded attachment Last edited by: Oreca at: 4/12/2016 6:42:19 PMLast edited by: Oreca at: 4/12/2016 6:50:59 PMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
5 thankful Users |
4/12/2016 6:41 PM | |
Joined: 3/14/2008 Last visit: 7/25/2024 Posts: 2079 Rating:
|
Thanks! Microman. The first thing I did when working with the APL default library was changing the extended status display so that the valves would not turn anymore. I thought this was very annoying, but made sense until I met a color blind operator. This is basically listed in the ISA papers as well (can't remember which one). See my previous post where I added an attachment for the icon numbers. |
Last edited by: Oreca at: 4/12/2016 6:45:53 PMIf I could help you, you can use the RATE button. Thank you. |
|
4/12/2016 6:49 PM | |
Joined: 3/14/2008 Last visit: 7/25/2024 Posts: 2079 Rating:
|
Yeah, that also a possible solution. I know the block icons numbers 3 and 4 (non rotating), with the black lines on both side is used to display a two way valve. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on